{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the replacement lens for the 9001KXPB and 9001KXTD pilot lights?
Issue:
Replacement lens for 9001KXPB and 9001KXTD part numbers

Product Line:
Pushbuttons and Operator Interface

Environment:
9001KXPB and 9001KXTD Square Operator

Resolution:
The replacement lens part number is 9001KXAC28. This comes with one clear cover, 5 color inserts and 2 blank legends (9001KXN200).  If the same color is required for position #1 and #2 of the KXPB operator, order 2 of Type KXAC28.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: