{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the size of the transition section from 5/15kV Outdoor NEMA 3R HVL switchgear to Masterclad metal clad switchgear?
Issue:
Size of the transition section from 5/15kV Outdoor NEMA 3R HVL switchgear to Masterclad metal clad switchgear

Product Line:
Masterclad/Metalclad switchgear

Environment:
Application

Resolution:
The transition is done in the rear of the HVL switch. The HVL enclosure is extended to be 80" deep. A 3" collar is used between the HVL section and the metal clad section. These units are front aligned. It can also be done with a 22" wide transition and a 3" collar.

Schneider Electric Canada