{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the highest ampere rating of EDB, EGB, and EJB breakers?
Issue:
What is the maximum current rating of an EDB breaker?

Product Line:
Molded Case Circuit breaker

Resolution:
The maximum amperage rating of EDB, EGB, and EJB breakers is 70 A for 1 pole and 125 A for 2 pole and 3 pole.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.