{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What size is the switch/fuse viewing window for the 5/15kV HVL switch enclosure? How high is it from the floor?

Issue:
Size and high from the floor of switch/fuse viewing window for the 5/15kV HVL switch enclosure

Product Line:
HVL/CC MV switchgear

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
The viewing window is 5.5" high and 21.5" wide. The center line of the window is 67.5" from the floor for indoor. Add 4" for NEMA 3R base channel. For inverted switches the center line of the window is 41" from the floor for indoor. Add 4" for NEMA 3R base channel.

Revised 01/14/09.

Schneider Electric Canada