{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is replacement coil part number 31002-400-40 still available?

Issue:
Identify a coil part number for a hoist contactor

Product Line:
Class 8965 Hoist Contactors

Environment:
NEMA Contactors and Starters

Resolution:
This was the original coil part number used in the old Class 8965 Types RO1, 2, 3, 4, 5, 6 reversing hoist contactors. These old reversing hoist contactors have long since been replaced by the Class 8965 Type RO10, 11, 12, 13.

Part Status: Obsolete - Use 31002-403-40 as a direct replacement. This part number includes TWO coils plus the jumper wire.

All Hoist contactors and accessories have been obsoleted. Suggest changing to LC1D

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: