{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are low consumptions coils available for the TeSys D Everlink offer?
Issue:
Is a Low Consumption DC Coil Available for the LC1D Contactor with the Everlink™ Connection?

Product Line:
IEC Contactors and Starters

Environment:
Tesys D Contactors

Resolution:
No. However the DC coils for the Everlink ( or LC1D..A) contactors do have a lower consumption (19w inrush and 7.4w sealed) than the older DC coils.

Schneider Electric Canada