{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 480Y/277V rated EMA SPD be used on a 120/208V system?
Issue:
Is it possible to use a 480Y/277V rated EMA SPD on a 120/208V system?

Product Line:
TVSS/ SPD

Environment:
Application

Cause:
Verification

Resolution:
No, the clamping voltage of the EMA SPD would be too high to be effective. Using a SPD designed for 480Y/277V on a 208Y/120V system would not allow it to provide adequate protection. A 208/120V SPD would start conducting at 150V from L-G and L-N, whereas a 480/277V SPD would start conducting at 320V from L-G and L-N. Additionally, placing a 480/277V SPD into a 208/120V system would cause issues with the diagnostics due to insufficient voltage for the diagnostic circuit.


Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: