{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement reset button for a Model 6 MCC, (Motor Control Center), Size 1 and Size 2 FVNR ( Full Voltage Non Reversing) and FVR ( Full Voltage Reversing) starters?
Issue:
Replacement reset button for a Model 6 MCC Size 1 and Size 2  FVNR and FVR starters

Product Line:
Model 6 MCC

Environment:
Maintenance

Cause:
Replacement

Resolution:
The reset Button is part number 80420-831-51 , but Reset Button part number does NOT include the gasket, p/n 29206-30700, or the retaining nut,  p/n 80439-680-01. These need to be ordered separately, if needed.

Schneider Electric Canada