{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a HOM2175SB or HOM250PSPD be used in a GE panelboard or load center?

Issue:
Can a HOM2175SB or HOM250PSPD Surge Breaker be used in a GE panelboard, or load center?

Product Line:
Surge Protective Devices

Environment:
Application

Cause:
Installation

Resolution:
No. Schneider Electric products are only designed, listed, and tested to be used only Square D Homeline load centers. An alternative solution for this application would be to use a GE 20A breaker to connect an HEPD25 , HEPD50 , or HEPD80 nipple mounted surge protective device. For flush mount applications you would need to also purchase the HEPD25MKF flush mounting kit if you choose to use the HEPD25. If you use either the HEPD50 or HEPD80 then you will need to use the HEPD58MKF flush mounting kit.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: