{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the H60XFA, H60XFA1212, H100XFA, H100XFA1212, H225XKA, H225XKA1212, H225XJG, or H225XJGAA be used for an outdoor, rainproof application?
Issue:
Application

Product Line:
Type 7/9 Enclosed Molded Case Switch

Resolution:
Yes, these devices are provided with a breather and drain kit (PKDB1) that can be field installed. When the PKDB1 is installed in the top and bottom end walls of the enclosure, the devices are suitable for an outdoor, rainproof application.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: