{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of the MDGF ground fault interface module S48891?
Issue:
Dimensional information on S48891 ground fault interface module.

Product Line:
Ground fault devices

Environment:
Product Specification

Resolution:
The MDGF Dimensions are: 4.17in (106.0 MM) W x 3.54in (90 MM) H x 2.28in (58.0 MM) D, 35 mm DIN rail mountable.


Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: