{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type and amperage primary fuses are used in MCC starter units with control transformers?
Issue:
Is there a fuse rating recommendation for Primary fuses used with 480V and Control tranformers (CPT) in Motor Control center starter buckets?

Product Line:
Motor Control Centers

Environment:
Application

Cause:
Clarification

Resolution:
The Primary fuses are FNQ-R type and recomended amperage per VA are listed below:
480V 50VA CPT-  1/4 amp P/N 25430-20025
480V 100VA CPT- 1/2 amp P/N 25430-20050
480V 150VA CPT- 1 amp P/N 25430-20100
480V 300VA CPT- 1 6/10 amp P/N 25430-20161
480V 500VA CPT- 2 8/10 amp P/N 25430-20281

Schneider Electric Canada