{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the ABL Power Supplies UL Class 2 rated?
Issue:
Does Schneider offer a class 2 rated power supply?

Product Line:
Phaseo DC Power Supply

Environment:
Power Supplies

Cause:
Product Specification

Resolution:
No they are not. The ABL7RM1202 and ABL7RM2401 are protection class conforming to VDE 01061: Class II without ground terminal (double insulated); this is an European standard only. There is no protection class for the ABL7RE devices. See the Phaseo catalog, document 8440CT0601 for details on specific parts.

Schneider Electric Canada

Attachment(s)
8440CT0601.pdf [2.69 MB]