{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a 9001KY3 available with an extra conduit entry in the top?
Issue:
Checking if the 9001KY3 enclosure is available with an extra conduit entry in the top

Product Line:
Push Buttons and Operator Interface

Environment:
9001KY/SKY Control Stations

Cause:
Need clarification before control station is installed.

Resolution:
No, the 9001KY enclosures have a bottom conduit opening standard. Extra conduit openings are not available.

Schneider Electric Canada