{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there any replacement deadfronts available for the NQ and NF panelboards with metal twistouts in the circuit breaker slots?
Issue:
Can the Series 1 (2008 and previous) NF Panelboard interior deafronts be replaced

Product:
NQ/NF Panelboards

Environment:
Maintenance

Cause:
Replacement

Resolution:
ONLY Load centers have twist out breaker deadfront feature and NQ and NF Panels currently do not. Plastic filler plates are ordered to fill un-used spaces with replacement interior deafronts for the NQ and NF Panelboards.



Schneider Electric Canada