{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the coil voltage codes for the LC1F800 contactors?
Issue
Coil Voltage suffixes on LC1F800 Contactor?

Product Line:
IEC Contactors and Starters

Environment:
Tesys F line Contactors and Accessories

Resolution:
AC and DC coil voltage codes for the LC1F800 (includes built in surge suppressor) are as follows:
FW is 110, 120 and 127 volts
MW is 220 and 240 volts
QW is 380, 415 and 440 volts

Schneider Electric Canada