{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do ANY of the general duty, heavy duty, or double throw safety switches contain knockouts in the enclosure?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches

Resolution:
GENERAL DUTY:
ALL 30 - 200 A, both NEMA 1 and NEMA 3R switches will contain knockouts in the enclosures
ALL 400 A, both NEMA 1 and 3R and ALL 600 and 800 A NEMA 1 only switches will contain knockouts in the enclosures

HEAVY DUTY:
ALL 30 - 200 A, NEMA 1, 3R, and 12K switches will contain knockouts in the enclosures

DOUBLE THROW:
ALL 30 - 200 Amp, NEMA 1 and NEMA 3R switches will contain knockouts in the enclosures

Schneider Electric Canada