Product Line:
Circuit Breakers
PowerPact H and J
Resolution:
The part number is 21590-20241.
NOTE:
It is a pan head steel thread forming trilobe screw with combination slot #3 square recess drive, ANSI specification SPECIFICATION: B18.6.4, size: 1/4-20, length : .75 +.00/-.03
Circuit Breakers
PowerPact H and J
Resolution:
The part number is 21590-20241.
NOTE:
It is a pan head steel thread forming trilobe screw with combination slot #3 square recess drive, ANSI specification SPECIFICATION: B18.6.4, size: 1/4-20, length : .75 +.00/-.03
Released for:Schneider Electric Canada