{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the threaded cover mounting screws on a Model 6 Motor Control Center? This is for the top and bottom wireway covers only
Issue:
Part number for the threaded cover mounting screws on a Model 6 Motor Control Center

Product Line:
MCC

Environment:
Model 6 MCC cover

Resolution:
The catalog number for the 10/32 x 1.25`` hex head gold anodized screw is: 8045022701

Schneider Electric Canada