{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the rail extensions provided with the Series D2 replacement QMB switches, such as QMB323TD?
Issue:
Do rail extensions for the Series D2 QMB switches, such as QMB323TD, need to be ordered separately?

Product Line:
QMB Panelboards

Environment:
Maintenance

Cause:
Clarification

Resolution:
The Rail extensions are provided and shipped with all series D2, QMB switches.

QMB

Schneider Electric Canada