{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the wire range for the sub-feed lug kits, NQSFL1 , NQSFL2 and NQSFL4 ?
Issue:
Wire range for Sub-Feed Lug kits NQSFL1, NQSFL2 and NQSFL4

Product Line:
NQ panelboards and accessories

Environment:
Product Features

Cause:
Determination of conductor size for specific sub-feed lug kits.

Resolution:
The below table shows the terminal data for the incoming and outgoing wires. See instruction bulletin,80043-729-01or 80043-745-01
AmpCatalog #IncomingOutgoing
100NQSFL1one #6-2/0 Al or Cuone #6-2/0 Al or Cu
225NQSFL2one 1/0-350 kcmil Al or Cuone 1/0-350 kcmil Al or Cu
400NQSFL4one 1/0-750 kcmil Cu onlyone 1/0-750 kcmil Cu only


Schneider Electric Canada