Search FAQs
What is the difference between the 9421LW1 and the 9421LW4 kits for the PowerPact M and P frame breakers?
Issue:
Characteristics of the 9421LW1 and the 9421LW4 kits for the PowerPact M and P frame breakers
Product Line:
Class 9421 Circuit Breaker Operational Mechanism, Powerpact M and P Frame
Environment:
Square D Operation Mechanisms
Resolution:
These kits consist of the following parts:
9421LW1 = 9421LW7 (opmech) + 9421LS8 (short shaft) + 9421LHP8 (handle)
9421LW4 = 9421LW7 (opmech) + 9421LS10 (long shaft) + 9421LHP8 (handle)
Characteristics of the 9421LW1 and the 9421LW4 kits for the PowerPact M and P frame breakers
Product Line:
Class 9421 Circuit Breaker Operational Mechanism, Powerpact M and P Frame
Environment:
Square D Operation Mechanisms
Resolution:
These kits consist of the following parts:
9421LW1 = 9421LW7 (opmech) + 9421LS8 (short shaft) + 9421LHP8 (handle)
9421LW4 = 9421LW7 (opmech) + 9421LS10 (long shaft) + 9421LHP8 (handle)
Item | Description |
1 | Operating mechanism |
2 | Handle assembly |
3 | Shaft |
4 | Shaft support bracket |
5 | Screw, #10-32 x 4-1/2 |
6 | Screw, 1/4-20 x 1/2 |
7 | Washer, 1/4 |
8 | Screw, #8-32 x 3/8 |
9 | Hex-head screw, 1/4-20 x 7/8 |
10 | Lock washer, 1/4 |
11 | Nut, 1/4-20 |
12 | Hex-head screw, 1/4-20 x 1/2 (self-tapping) |
13 | Screw, 1/4-20 x 3/4 (self-tapping) |
14 | Handle gasket |
A | Interlock pin location |
B | Actuator |
C | Circuit breaker |
D | Enclosure door |
E | Panel |
H | Mounting depth |
L | Shaft length |
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: