Issue:
What is the meaning of Form R172 when used as a suffix on a starter catalog number?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Contactors and starters
Resolution:
Form R172 used to be a Form for addition of a two pole control relay. R172 is now obsolete, and is replaced by form R174 which will add a four pole relay.
What is the meaning of Form R172 when used as a suffix on a starter catalog number?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Contactors and starters
Resolution:
Form R172 used to be a Form for addition of a two pole control relay. R172 is now obsolete, and is replaced by form R174 which will add a four pole relay.