{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the consumption of the control coil for Class 8502 or 8536 Type SB contactor / starter?
Issue:
Identifying consumption of the coil in a NEMA size 0 contactor or starter

Product Line:
NEMA Contactors and Starters

Environment:
8502/8536 Type S Contactors and Starters

Cause:
Identifying consumption of NEMA size 0 device

Resolution:
245 VA inrush and 27 VA sealed for 60 hertz or 232 VA inrush and 26 VA sealed for 50 hertz.

This also applies to all 8538SB, 8539SB, 8606SB, 8630SB, 8640SB, 8702SB, 8736SB, 8738SB, 8739SB, 8810SB


CTA-ID : 2052404

Schneider Electric Canada