{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does an 8430MPSV24 or an 8430MPSV29 phase failure relay have overvoltage protection?
Issue:
Over voltage protection for 8430MPSV24 or an 8430MPSV29 phase failure relays

Product Line:
Relays and Timers

Environment:
Zelio Phase Measurement Relays

Resolution:
No. Although this relay can tolerate up to a 10% overvoltage level, it is normally used for phase failure protection only. For overvoltage protection we would recommend an IEC relay catalog number RM17TE00. It has a settable voltage window for overvoltage and under-voltage.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: