{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there sufficient depth in a 9001KYK enclosure to stack 9001KA contact blocks?
Issue:
Is there sufficient depth in a 9001KYK enclosure to add an additional 9001KA contact block?

Product Line:
Type B and 30 mm Control Stations

Environment:
Pushbutton and Operator Interface

Resolution:
According to the 9001 Specifiers Guide, enclosures have sufficient depth to accommodate two contact blocks in tandem (total of four blocks) on non-illuminated operators and two contact blocks side-by-side on illuminated operators.

Schneider Electric Canada