{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is sprinkler proof bus duct available from Square D by Schneider Electric?

Issue:
Sprinkler proof busway selection

Product Line:
I-Line Busway

Environment:
Products sold in North America

Resolution:
Yes it is available but only with the 800A to 5000A I-Line II series busway product.
IP54 rated busduct will withstand sprinklers. We must density rate the bus bars to receive UL approved product.
IP54 construction is not available for 225 thru 600A busway products.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: