{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the Homeline branch breakers classified (or does Square D authorize them) to be used in competitors load centers?
Issue:
Product Design Features

Product Line:
Homeline Branch Breakers

Resolution:
NO. The Homeline branch breakers are NOT classified to be used in competitors load centers. Also, the use of the branch breakers in competitors load centers is NOT authorized by Square D.

Schneider Electric Canada