{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Adding a CE3200E to an existing CDP panel

Issue:
Obsolete breaker

Product Line:
Circuit breakers


Resolution:
The CE3200E breaker is obsolete.
The Replacement breaker is a Square D JGL36200 breaker with a JDCMH mounting kit. This breaker is rated 18KAIC at 600V.
The JDCMH will mount two J frame breakers.
An S37445 is included in the JDCMH to convert breaker from Lug-Lug to Lug-Pad. If a second breaker is being mounted on the JDCMH Hardware, order an additional S37445.
Hardware Kit requires both sides of panel and will only mount Powerpact H Breakers.


Schneider Electric Canada

Attachment(s)

JDCMH 32-02-211a-00x.pdfJDCMH 32-02-211a-00x.pdf [123.67 KB]