Search FAQs
What are the replaceable parts for the 2510KW2H manual starter?
Issue:
Replacement parts available for 2510KW2H
Product Line:
Class 2510 Manual Starters
Environment:
NEMA Contactors and Starters
Resolution:
The Series A, Class 2510 Type KW2H, NEMA 4, watertight device, was obsoleted January of 2002 and replaced by the Class 2510 KW2H Series B.
Series B consists of a redesigned enclosure (box) and cover assembly. The physical size of the new Series B is almost identical to the Series A except for the overall width of the enclosure (box) is slightly wider - wider by only .15" (5/32"). The mounting holes for the Series B device are identical to the old Series A device.
Series A covers and boxes are NOT interchangeable with Series B devices due to the redesign. This is due to changes in location of the four (4) cover mounting screws.
Replacement parts available for 2510KW2H
Product Line:
Class 2510 Manual Starters
Environment:
NEMA Contactors and Starters
Resolution:
The Series A, Class 2510 Type KW2H, NEMA 4, watertight device, was obsoleted January of 2002 and replaced by the Class 2510 KW2H Series B.
Series B consists of a redesigned enclosure (box) and cover assembly. The physical size of the new Series B is almost identical to the Series A except for the overall width of the enclosure (box) is slightly wider - wider by only .15" (5/32"). The mounting holes for the Series B device are identical to the old Series A device.
Series A covers and boxes are NOT interchangeable with Series B devices due to the redesign. This is due to changes in location of the four (4) cover mounting screws.
Description: | Original P/N Ser A: | Replacement P/N Ser B: |
Replacement Toggle Kit | 9998HW1 | 9998HW1 |
Cover Gasket | Obsolete (see note 1) | 31056-081-01 |
Box (back portion of enclosure) | Obsolete (see note 2) | 31056-080-51 |
Cover Complete | Obsolete (see note 3) | 31057-529-52 (see note 4) |
Toggle Type Switch (3 Pole) | 2510KO2 | 2510KO2 |
Notes:
1. If the Cover Gasket on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
2. If the Box on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
3. If the Cover on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
4. The Cover Complete includes the Cover Gasket (31056-081-01).
1. If the Cover Gasket on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
2. If the Box on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
3. If the Cover on a Series A device requires replacement, a Series B Cover Complete and Box MUST be ordered. None of these parts are interchangeable between series.
4. The Cover Complete includes the Cover Gasket (31056-081-01).
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: