Search FAQs
Can the cover on the J250R circuit breaker enclosure be padlocked?
Issue:
Padlock for the cover of J250R
Product Line:
Circuit Breaker Enclosure
Resolution:
Yes, the cover actually has two places for a padlock. The enclosure cover can be padlocked to prevent access to the enclosure interior. There is also a smaller plastic cover located on the enclosure cover that provides access only to the circuit breaker operating handle that can also be padlocked closed.
Padlock for the cover of J250R
Product Line:
Circuit Breaker Enclosure
Resolution:
Yes, the cover actually has two places for a padlock. The enclosure cover can be padlocked to prevent access to the enclosure interior. There is also a smaller plastic cover located on the enclosure cover that provides access only to the circuit breaker operating handle that can also be padlocked closed.
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: