{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 9422A4 handle be used in place of the 9422A2 handle
Issue:
Are 9422A2 and A2 interchangeable?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Handle Mechanisms

Resolution:
Not in all cases. While both have the same mounting dimensions, the 9422A4 handle is 2` shorter than the 9422A2 handle . Since this is a 4`` handle it is not recommended for use with 100A and 200A disconnect switches or LAL and larger circuit breaker operating mechanisms.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: