{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the Form M10 designate for a NEMA starter or contactor?
Issue:
Identify the meaning of a form in a NEMA contactor part number

Product Line:
Class 8502 Contactors and Starters

Environment:
Square D Contactors and Starters

Resolution:
M10 indicates Marine Control. This is a modification of a standard NEMA 4 or 12 device for use as Marine control per UL508 Marine supplement SA (Industrial Control Equipment for Marine use (February 23, 1993) and CFR46 (Subchapter J - Electrical Engineering 10-1-93 edition.)

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: