{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the melting alloy overload block be replaced on 8911DPSO12, or 8911DPSG12 Definite Purpose Starters?
Issue:
Replacing the melting alloy overload block for 8911DPSO12 or 8911DPSG12

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8911 Definite Purpose Starters

Cause:
Replacement overload needed

Resolution:
No. The overload section of 8911 Definite Purpose Contactors is not replaceable because it has a special bussing arrangement that connects it to the contactor. Customer can use a separately mounted overload or buy a new starter.


Schneider Electric Canada