{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can additional neutral bars be added to the NQ or NF panelboards?

Issue:
Are field installable neutrals available

Product Line:
NQ / NF Panelboards

Environment:
Products sold in North America

Resolution:
There are no field installable neutral bars available for the NQ or NF paneboards.
The neutrals that come installed with these panels are properly sized for the circuit count and amperage of the specific panel. Add on lugs are available.

Schneider Electric Canada