Search FAQs
Are auxiliary contacts available for 8965RO12?
Issue:
8965RO12 Auxiliary contacts used
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8965 Reversing Hoist contactors
Resolution:
Yes, order the 9999R10 for normally open or 9999R11 for normally closed. The contact blocks mount between the foward and reversing contactors. You can only install 1 contact block per 8965RO10 device. The 9999R blocks actually contain either 2 NO or 2 NC contacts in the module, one for each side of the device.
8965RO12 Auxiliary contacts used
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8965 Reversing Hoist contactors
Resolution:
Yes, order the 9999R10 for normally open or 9999R11 for normally closed. The contact blocks mount between the foward and reversing contactors. You can only install 1 contact block per 8965RO10 device. The 9999R blocks actually contain either 2 NO or 2 NC contacts in the module, one for each side of the device.
Released for:Schneider Electric Canada
Explore more
Product:
Range:
Explore more
Product:
Range: