Issue:
Storage temperature for 8502/8536 Starters
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 NEMA Contactors and Starters
Resolution:
Per NEMA standards, the storage temperature rating for NEMA rated devices is -30 degrees C to 65 degrees C. If the equipment is to be stored for more than 1 week, it may be necessary to cover the equipment and provide a source of heat to prevent condensation.
This rating also applies to 2510, 8538, 8539, 8606, 8630, 8640, 8702, 8736, 8738, 8739, 8810, 8903, 8940 and 8941 devices.
Storage temperature for 8502/8536 Starters
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 NEMA Contactors and Starters
Resolution:
Per NEMA standards, the storage temperature rating for NEMA rated devices is -30 degrees C to 65 degrees C. If the equipment is to be stored for more than 1 week, it may be necessary to cover the equipment and provide a source of heat to prevent condensation.
This rating also applies to 2510, 8538, 8539, 8606, 8630, 8640, 8702, 8736, 8738, 8739, 8810, 8903, 8940 and 8941 devices.
Released for:Schneider Electric Canada