{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are all definite purpose contactors 120 Amp and larger, including 8910DPA122, DPA123, SYD138, SYD230 and SYD368 obsolete? What is the recommended replacement?
Issue:
Replacing definite purpose contactors above 90 amps

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8910 Definite Purpose contactors

Resolution:
Yes, these higher amperage definite purpose contactors have been obsoleted.
The transition devices will be either the NEMA Type S contactors or the TeSys D and F contactors.

Schneider Electric Canada