{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a hand off auto selector switch available on a 2510 Type M manual starter?
Issue:
HOA selector switch for the 2510 type M manual starters

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510 Type M Manual Starters

Cause: Would like a hand off auto selector switch for a 2510M manual starter

Resolution:
No, a hand off auto is not offered for the 2510 type M manual starters. Hand Off Auto is normally available only on electrically held devices.

Schneider Electric Canada