{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the operating temperature rating for the SSRP Solid State Relays? Also, when is a heat sink required?
Issue:
Temperature Rating of the SSRP Relay with and without the Heat Sink

Product Line:
Relays and Timers

Environment:
SSRP Solid State Relay

Resolution:
-40 degrees C to + 80 degrees C = operation; -40 degrees C to +125 degrees C = storage and any unit that does not have a heat sink built in needs a heat sink or thermal interface (pad) to dissipate the heat that is generated.

Schneider Electric Canada