{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the coil consumption of a 8501 Type K relay?
Issue:
Needs to know the coil consumption of a 8501 Type K relay.

Product Line:
Push Buttons and Operator Interface

Environment:
Class 8501 Relay

Resolution:
For the Types KP , KU , and KF AC 3.6 VA inrush and 2.5 VA sealed.
For the Types KPD , KUD, and KFD 1.5 watts standard, and 3 watts maximum.
For the Type KL AC 2.0 VA to latch and 0.8VA to unlatch.
For the Type KLD 1.2 watts to latch and unlatch.
For the Type KX AC 3.7VA inrush 2.7VA sealed
DC 1.2 watts standard, 3 watts maximum

Schneider Electric Canada