{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for a coil part number 31002-400-19 ?
Issue:
Coils for old Class 8965 Types RO1, 2, 3, 4, 5, 6.

Product Line:
Reversing Hoist Contactors

Environment:
Class 8965 Types RO1, 2, 3, 4, 5, 6.

Resolution:
This 31002-400-19 coil was the original coil part number used in the old Class 8965 Types RO1, 2, 3, 4, 5, 6.  These old reversing hoist contactors have long since been replaced by the Class 8965 Type RO10, 11, 12, 13. Use 31002-403-19 as a direct replacement for the 31002-400-19. This part number includes TWO coils plus the jumper wire.

Schneider Electric Canada