{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 8536 starter be mounted horizontally?
Issue:
Need to mount the 8536 starter horizontally/ Is it possible?

Product Line:
8536S Starters

Environment:
NEMA Contactors and Starters

Cause:
Needs to verify if a 8536 starter be mounted horizontally.

Resolution:
The type S starters (melting alloy type only) s1zes 0 through 4 can be mounted horizontally or vertically in the vertical plane. They cannot be flat mounted against a ceiling or laid on the floor of an enclosure.
Type S lighting contactors have additional restrictions.

Schneider Electric Canada