{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider Energy Efficient transformers meet TP-2?
Issue:
Do Square D Energy Efficient Low Voltage Transformers meet TP-2?

Product Line:
Transformers

Environment:
Energy Efficient Low Voltage Transformers

Resolution:
Our ventilated transformers meet TP-1, TP-2 and TP-3.
TP-1 Defines the NEMA standard defining the energy efficiency performance of transformers.
TP-2 Defines the test procedures for meeting the requirements of TP-1
TP-3 Defines the labeling of transformers tested to the efficiency levels specified in TP-1.

Schneider Electric Canada