{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a MA36600 breaker be mounted in a HCP-SU type panel?
Issue:
Will a 600A breaker fit into a HCP-SU type panel?

Product Line:
Panelboards

Environment:
I line Power Distribution Panelboards

Cause:
Compatibility

Resolution:
The Panel's interior will accept the MA, MH breakers but they are obsolete and NLA. The MGA36600/MJA36600 will directly mount into its' space.
Along with 600A MG/MJ breakers, the MGA36800/MJA36800 800AT/800AF breakers and PG/PJ/PL  800AT/1200AF breakers will also mount into
the HCP-SU interior .

Schneider Electric Canada