{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the complete pushbutton kit for a 2510MBA manual starter?
Issue:
Pushbutton kit for a 2510MBA

Product Line:
Type M and T Integral Horsepower Starters

Environment:
Manual Starters / Protectors

Resolution:
The part number is 31085-986-50. It consists of:
Quanity (1) 31085-381-50 pushbutton assembly.
Quanity 1- 29206-30840 o-ring for the pushbutton assembly
Quanity (6) 21506-04140 pushbutton assembly mounting screws #4-24x 7/16``.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: