Issue:
Field asemble reversing contactor
Product Line:
IEC Contactors and Starters
Environment:
Tesys D Reversing Contactors
Resolution:
(2) LC1DT20 - 40 contactors and (1) LADT9R1V mechanical interlock kit. Note: Mechanical interlock kit includes power bus reversing connections and electrical interlock bus. It is important to note that the electrical bus is of a size to couple the two devices together and prevent vibration from separating them. Thus, even though smaller wires can carry the current load, they are not recommended as this bus forms part of the structure of the completed assembly.
Field asemble reversing contactor
Product Line:
IEC Contactors and Starters
Environment:
Tesys D Reversing Contactors
Resolution:
(2) LC1DT20 - 40 contactors and (1) LADT9R1V mechanical interlock kit. Note: Mechanical interlock kit includes power bus reversing connections and electrical interlock bus. It is important to note that the electrical bus is of a size to couple the two devices together and prevent vibration from separating them. Thus, even though smaller wires can carry the current load, they are not recommended as this bus forms part of the structure of the completed assembly.