Search FAQs
Will the LC1D093G7 accept the standard LRD08 overloads?
Issue:
Overload relay for a spring terminal contactor
Product Line:
IEC contactors and starters
Environment:
Tesys D Contactors and Overload relays
Resolution:
No, for the LC1D093 spring terminal version contactor , you will need to add the 3 to the end of the LRD overload. ie: An LRD08 will become a LRD083.
Overload relay for a spring terminal contactor
Product Line:
IEC contactors and starters
Environment:
Tesys D Contactors and Overload relays
Resolution:
No, for the LC1D093 spring terminal version contactor , you will need to add the 3 to the end of the LRD overload. ie: An LRD08 will become a LRD083.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: