Search FAQs
What is the difference between th 9007MS10G0300 and 9007MS10S0300 limit switches?
Issue:
Checking on the difference between part numbers 9007MS10G0300 and 9007MS10S0300
Product Line:
9007MS Miniature Limit Switches
Environment:
NEMA Limit Switches
Resolution:
The (G) in the 9007MS10(G)0300 represents gold contacts and the (S) in 9007MS10(S)0300 has 10A silver contacts, which are more durable and more widely used. Gold contacts are used in very low current applications, or in corrosive environments where cycling is very infrequent.
Checking on the difference between part numbers 9007MS10G0300 and 9007MS10S0300
Product Line:
9007MS Miniature Limit Switches
Environment:
NEMA Limit Switches
Resolution:
The (G) in the 9007MS10(G)0300 represents gold contacts and the (S) in 9007MS10(S)0300 has 10A silver contacts, which are more durable and more widely used. Gold contacts are used in very low current applications, or in corrosive environments where cycling is very infrequent.
Released for:Schneider Electric Canada
Explore more
Category:
Range:
Explore more
Category:
Range: