Search FAQs
What UL File numbers are the B Hubs covered under, like the B150, B200, B250, B300, etc?
Issue:
Product Design Features
Product Line:
B Type Hubs
Resolution:
Below are the UL File numbers that all the B Type Hubs are listed under.
UL File Number E58678 for the following B Hubs:
B300
B350
B400
UL File Number E4709 for the following B hubs:
B075
B100
B125
B150
B200
B250
Product Design Features
Product Line:
B Type Hubs
Resolution:
Below are the UL File numbers that all the B Type Hubs are listed under.
UL File Number E58678 for the following B Hubs:
B300
B350
B400
UL File Number E4709 for the following B hubs:
B075
B100
B125
B150
B200
B250
Released for:Schneider Electric Canada
Explore more
Category:
Explore more
Category: